Technical FAQs

Ask a Question

Does Schneider Electric offer the belt clamps for LM-P/S 608 , part number 743200870106 ?

Yes, 743200870106 is available through our service.sales department

Send an email to

In the email text make sure you state that you wish to order "Berger Lahr" spare part of : Set of belt take up LM-P/S608R/K AT5 - order number 0074320870106

Include your contact phone number and return email address to that someone from that department can contact you with pricing and delivery information.

Was this helpful?
What can we do to improve the information ?