Technical FAQs

Ask a Question

Is there a way to set an alarm when there is a communication error with Vijeo Designer?

You can use the @sys:2.  When there is a communication packet error or communication timeout the bit is set to 1.  When the communication is good the bit is 0.
Was this helpful?
What can we do to improve the information ?