Technical FAQs

Ask a Question

Why are all my projects missing in the Vijeo-Manager in the navigator of Vijeo Designer?

There is a file in the Vijeo-Manager that generates the projects called Info.IFM. Delete this file and re launch Vijeo Designer as the projects should reappear again. It could be that the Info.IFM file is corrupted.

Vijeo Designer project paths:
V5.0 or lower -> under My Documents
 
V5.1 and higher
XP -> C:\Documents and Settings\All users\Shared Documents\Vijeo Designer\Vijeo Manager
Vista & 7 -> C:\Users\Public\Public Documents\Vijeo Designer\Vijeo Manager


 
 
 
Was this helpful?
What can we do to improve the information ?