Technical FAQs

Ask a Question

What is the thermal dissipation for the 499NES18100 ?

Title
Thermal dissipation for the 499NES18100 i
 
Issue
Customer needs thermal dissipation for the 499NES18100 i
 
Product Line
Connexium Switches, 499NES18100
 
Environment
499NES18100
 
Cause
N/A
 
Resolution
The thermal dissipation for the 499NES18100 is 7.0 watts maximum at 24 VDC. 
Was this helpful?
What can we do to improve the information ?