Technical FAQs

Ask a Question

Can the Vijeo Design'Air app connect to the Magelis over VPN?

Issue:
Can the Vijeo Design'Air app connect to the Magelis over VPN?

Product Line:
Vijeo Design'Air, Vijeo Designer

Environment:


Cause:


Resolution:
Yes, Vijeo Design'Air app supports VPN connections to the Magelis.  But PPTP only.
Was this helpful?
What can we do to improve the information ?