Technical FAQs

Ask a Question

Is it possible to delete an RIO or ERIO drop using CCOTF? (Change Configuration on the Fly)

No. You cannot delete a drop.

CCOTF will support the following actions.

RIO
 -Add a discrete or analog module in a free slot
- Delete a discrete or analog module
- Modify the configuration and adjustment parameters of a module

ERIO
-Add a Quantum or Modicon M340 EIO drop
-Add a discrete or analog module in a free slot
-Delete a discrete or analog module
-Modify the configuration and adjustment parameters of a module
Was this helpful?
What can we do to improve the information ?