Technical FAQs

Ask a Question

Not able to save changes to my UNITELWAY driver communication port settings.

First thing to check is the security permissions for the CnfUTW3.dat file in the Windows/System32 directory. Make sure that this file is set to allow (Full control, Modify, Read & execute, Read, Write and Special permissions.).  This file can also be manually modified with Notepad to reflect the new communication port settings required.  
Was this helpful?
What can we do to improve the information ?