Technical FAQs

Ask a Question

What is the meaning of an error 300A or 300B hex on my MSTR?

This error indicates an exception response from an Ethernet Bridge device. 0A hex indicates that the message could not find a path through the bridge. 0B hex indicates that the slave did not respond to the message..
Was this helpful?
What can we do to improve the information ?