Technical FAQs

Ask a Question

What would cause a 4000 hex error code on a Compact controller?

The 4000 hex is a traffic cop error stating that the I/O module mapped does not match the module in the slot. This can be also caused with the low end controllers that require a loadable for it to be mapped.
Was this helpful?
What can we do to improve the information ?