Technical FAQs

Ask a Question

I added a secondary SSD hard drive, part number HMIYSSDS080S1, in the Magelis S-Box iPC but Windows does not recognized the hard drive. How do I resolve the issue?

Issue:
I added a secondary SSD hard drive, part number HMIYSSDS080S1, in the Magelis S-Box iPC but Windows does not recognized the hard drive.  How do I resolve the issue?

Product Line:
S-Box, Panel PC, Box PC, Rack PC, Magelis iPC

Environment:


Cause:


Resolution:
The secondary hard drives for the Magelis S-Box does not come partitioned or formatted.  It is up to the End User to partition and format to their specifications.
Was this helpful?
What can we do to improve the information ?