Technical FAQs

Ask a Question

How to replace the obsolete limit switches XCMA1524569 and XCMA1524570?

Please note that the XCMA1524569 and XCMA1524570 specific switches are discontinued since 2005.
Both references are in fact XCMA102 limit switch (see attached picture) with adapted cable lenght
- XCMA1524569 = cable lenght of 33 cm (centimetre),
- XCMA1524570 = cable lenght of 63.5 cm.

Substitution by the standard XCMD2102L1 limit switch with 1m cable lenght.
Was this helpful?
What can we do to improve the information ?