Technical FAQs

Ask a Question

Can the Magelis HMIPPF7A2701 be mounted at a 45 degree angle?

The unit can be mounted at a 45 degree angle as long as the ambient air temperature does not exceed 85F and that there is enough air flow surrounding the unit.
 
Was this helpful?
What can we do to improve the information ?