Technical FAQs

Ask a Question

How to use LXM32M advanced setting in SoMachine?

In Somachine we add the device on CanOpen tree. We have two option for same device.
For example, Lexium 32M or Lexium 32M advanced setting.
The difference is the DTM available in Lexium 32M advanced setting.Then we don't need connect drive to PC.
When Somachne is online, we can modfiy the parameter in SoMachine.
The detail you can see the attachment.
Was this helpful?
What can we do to improve the information ?