Technical FAQs

Ask a Question

How to combine the XY2C (E.stop rope pull s/w) with XPSAF5130 safety relay?

You can combine XY2CH/CE/CJ E.stop rope pull switch to the XPSAC unit or to the XPSAF5130 unit, like shown in the attached diagram or in the XPSA* instruction sheet.

For the XPSAF5130, it is the standard wiring diagram to use : in the instruction sheet, you replace the E.stop mushroom by the XY2C* rope pull switch to get a PLe category 4 application by using XY2C* model with 2 NC contacts, so XY2CH1xx7x ref or XY2CExxx7x ref. See attached file showing example.

Was this helpful?
What can we do to improve the information ?