Technical FAQs

Ask a Question

What is the communication cable between the XBTR411 and the M221 controller (Modbus RS485)?

The XBTZ938 communication can be used between the XBTR411 and the M221 SoMachine basic controller.
Was this helpful?
What can we do to improve the information ?