Technical FAQs

Ask a Question

Proworx 32 error "Invalid bands collection index (2007)"

Issue:
   This error is displayed when launching Proworx 32.

Resolution:
  Close Proworx 32 and delete the layout3.acf file and relaunch Proworx 32.
Was this helpful?
What can we do to improve the information ?