Technical FAQs

Ask a Question

Is there a HMI with Wi-Fi capabilities

Yes.  The new Magelis HMIGTU 12" Display includes Wireless Lan capabilities.
The Innovative Access Point embedded in HMI to provide easy ,robust and secure wireless connection to Industrial architecture.
This Display is available only with the last version of Magelis GTU Open Box PV02/SV2.0 or later AND VijeoDesigner software version V6.2 SP3.
This unit will be available in June 2015.  The part number is HMIDT643.

Was this helpful?
What can we do to improve the information ?