Technical FAQs

Ask a Question

What is largest memory card size I can get for a Premium TSXH5724M?

Issue:
What is largest memory card size I can get for a Premium TSXH5724M?

Product Line:
TSX Premium

Environment:


Cause:


Resolution:
The TSX Premium TSXH5724M supports up to 768k of optional memory on a PCMCIA memory card.  If wish to use a memory card that provide the maximum memory, it is recommended that you use one of the following cards:
SRAM part number  is     TSXMRPC768K
EEPROM part number is TSXMFPP001M
note: you can use cards with larger memory size, however you are still limited to 768k of memory
Was this helpful?
What can we do to improve the information ?