Technical FAQs

Ask a Question

What causes Concept error "1052 - Failure reading Desktop file"?

Cause:
    This is caused because the format of the .dsk file has changed.   This file holds the adjustments, Concept options, and information about the screens.
It is possible that it was was left open when Concept was closed.

Resolution:
  • Delete the project's .dsk file and let Concept rebuild it.
  • If the error occurs when opening the project, delete project.dsk.
  • If the error occurs when  launching Concept, delete concept.dsk.
  • Make sure the _sa.ini file is not read only.

 
Was this helpful?
What can we do to improve the information ?