Technical FAQs

Ask a Question

Can Concept error '801 - error opening loadable file' be corrected?

Cause:
    Concept is unable to locate a loadable on the disk when doing a compare or download.

Resolution:
    Make sure the loadable used in the project resides on the "Installed" side of the Configure - Loadables section of the Configurator.

    If not, move if from the "Available" column on the left to the "Installed" column on the right.

    If it is not "Available", hit the <Unpack> button and point to the loadable's .EXE or .DAT file and <Unpack> it.  It will then
    show up in the "Available" column and can be "Installed".

    Make sure that all user loadables needed in the project are in the Concept \DAT folder.
    
Was this helpful?
What can we do to improve the information ?