Technical FAQs

Ask a Question

What is the RAL colour of the XY2CE* E.stop rope pull switches with reset button?

The casing of the XY2CE* E.stop rope pull switches with reset button is in zinc alloy material. It is painted in RAL3000 red colour, since June 2012.
When casing colour changed, the front face, in steel painted in the past, moved to stainless steel with new pilot light and reset button.
Was this helpful?
What can we do to improve the information ?