Technical FAQs

Ask a Question

What level of RAID is used in the Magelis Panel PC?

Issue:
What level of RAID is used in the Magelis Panel PC?

Product Line:
Magelis Panel PC, HMIPPH9, HMIPPF9, HMIPPH7, HMIPPF7

Environment:


Cause:


Resolution:
The Panel PC supports level 1 RAID (RAID 1)
Was this helpful?
What can we do to improve the information ?