Technical FAQs

Ask a Question

How do I wire a Schneider Electric 930 Ultrasonic sensor XX930A.A.0.M12 to a M221 controller?

BRN and BLU powers the sensor (15-25VDC)
BLK and WHT is the 0-10V signal to the PLC

The PLC has an analog input range or 0-10V.
BLK goes to AN Red on the M221
WHT goes to 0V Black on the M221

Was this helpful?
What can we do to improve the information ?