Technical FAQs

Ask a Question

How to enable Fault Record for a Micom P63x?

Issue:
When trying to review a fault there is no record of the fault in a Micom relay

Product Line:
MiCOM P63x

Environment:
MiCOM S1 Studio "Event"

Cause:
The fault recording is not enabled by default.

Resolution:
To enable fault recording open the P63x in MiCOM S1 Studio and open the settings file.  
Once the setting file is open navigate to to Parameters -> Function parameters -> Global ->FT_RC which is shown below. 

Double click on Fct. Assign. Trigger and the popup below will display.  Select what fault recording needed and click  configure.  Once all the faults are picked click ok.


 
Was this helpful?
What can we do to improve the information ?