Technical FAQs

Ask a Question

What is the Schneider Electric part number for ordering Berger Lahr IFS91 type motor with ID number 66109100037 ?

66109100037 is available from Schneider Electric using the new part number system.
Schneider has changed the ordering method for Integrated motors that have gearbox's 
Now the gearbox, gearbox mounting kit and motor are ordered as separate items.
This way the customer can order just the items they need.

Here are the part numbers to replace 66109100037.

Motor = ILS1F851PB1A0
Gearbox = GBX080008K
Adapter kit for mounting gearbox to motor = GBK0800852S
Was this helpful?
What can we do to improve the information ?