Technical FAQs

Ask a Question

Diagnostics Tool has stopped working in SPM 7.0.x/ PME7.2.x/ PME 8.0

The following message pops up when running the diagnostics tool in SPM 7.0.x/ PME 7.2.x/ PME 8.0 :

          Diagnostics Tool has stopped working
          check online for a solution and close the program
          close the program
          debug the program

Product Line
Power Monitoring Expert 8.0
Power Monitoring Expert 7.2.x
Struxureware Power Monitoring 7.0.x

Windows Server 2012 R2
Windows Server 2008 R2

User is logged in to the server with non-administrative rights.

Login to the server with a user within Administrators group.
Was this helpful?
What can we do to improve the information ?