Technical FAQs

Ask a Question

Does Schneider Electric offer a replacement for ILS1R851S1390 ?

ILS1R851S1390 is a special version for the OEM machine builder.
This particular model comes with a keyed shaft.  (The standard version has a smooth keyless shaft.)
This model also has a special version of firmware.

The customer should contact the OEM machine builder to get the exact replacement.
The OEM machine builder as a contract with the factory that this motor (ILS1R851S1390) is proprietary to them and not available for purchase to anyone except the OEM machine builder 

No other motor will be compatible as a replacement.
Was this helpful?
What can we do to improve the information ?