Technical FAQs

Ask a Question

Which operating systems is the Vijeo Designer Runtime compatible with?

Windows XP Embedded
Windows Embedded Standard 2009.
Windows 7 Embedded x32 and x64 systems
Windows XP Professional (Service Pack 3 or greater)
Windows 7 32 and 64 bit
Windows 8.1 32 and 64 bit

Was this helpful?
What can we do to improve the information ?