Technical FAQs

Ask a Question

Is there a print function available in SoMachine Basic?

Yes. As of April 2015 with SoMachine Basic software version 1.3 SP1 build 44532 you can now print.
as of 2/27/2017 the current version of SoMachine Basic is 1.5.
Was this helpful?
What can we do to improve the information ?