Technical FAQs

Ask a Question

What is the weight of a BPH1422N5MA2CA1 motor?

Issue:  None

Product Line: Lexium BPH

Environment: None

Cause: Shipping need

Answer:  BPH1422N5MA2CA1 is a Lexium BPH motor without a brake. Its approximately weight without brake is 17.2 Kg. With a brake included, the same motor would weigh approximately
20.1  Kg.
Was this helpful?
What can we do to improve the information ?