Technical FAQs

Ask a Question

"A valid software license could not be found" on Secondary Server

Issue
Not being able to add devices in Management Console in  PME on the Secondary server.  The following message pops up:

          

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.0

Environment
Secondary server

Cause
Trial license

Resolution
The system needs to be fully licensed in order to enable a secondary server.
Was this helpful?
What can we do to improve the information ?