Technical FAQs

Ask a Question

What is the replacement to the M580 BMXNOC0402 ethernet module?

Part# BMENOC0301 and BMENOC0311
These replacement BMENOC03•1 modules utilize the Ethernet backplane to allow direct Ethernet communication to the CPU. These new modules have advanced cyber security and robustness features that bring extra value to customers.
 
Was this helpful?
What can we do to improve the information ?