Technical FAQs

Ask a Question

What causes an '-850' error when downloading changes to the PLC in Concept?

Running out of available User Logic space in the PLC will cause this error.

-   Optimize the project offline and redownload or perform a full download.
-   Increase the IEC heap size in the PLC Configuration section of the project (offline).
-   Decrease the Global data in the PLC Configuration (offline)
Was this helpful?
What can we do to improve the information ?