Technical FAQs

Ask a Question

What causes Winsock error #10061 when attempting to use the Unity OS Loader?

This error is encountered if the Copro security settings are disabled. You need to enable each of these fields if you intend to flash the Copro or view the CPU's Web page.

Was this helpful?
What can we do to improve the information ?