Technical FAQs

Ask a Question

What causes the " password is not equal in application and in request" error when connecting to a PLC using Unity Pro software?

Issue:
   Error is displayed when trying to connect to a PLC using Unity Pro programming software.

Resoltuion:
   - Reflash the executive firmware in the PLC.
   - Is the version of the firmware specificied in the CPUs configuration compatible with the version of Unity Pro being used?
Was this helpful?
What can we do to improve the information ?