Technical FAQs

Ask a Question

Is it possible to use an ATV71 MFB (motion function blocks) eds file for an ATV61 in Unity Pro?

It is not possible to use an ATV71 MFB (motion function blocks) eds file for an ATV61 in Unity Pro. The ATV61 can be controlled via CANopen using with PDOs and SDOs and the appropriate eds file version that can be downloaded from www.schneider-electric.com. MFB (motion function blocks) like MC_Power, MC_Jog, etc cannot be used for an ATV61 in Unity Pro.
Was this helpful?
What can we do to improve the information ?