Technical FAQs

Ask a Question

Do Lexium Integrated Drives come with connectors that interface with the internal plugs?

No, Lexium Integrated Drives do not come with any of the plugs that mate with the internal connectors.
All mating plugs are available as an accessory and must be ordered separate

Even the Lexium Integrated Drive with Industrial Connectors do not come with the mating connectors to interface with the connections found on the industrial cover.
You must also order these mating connectors as an accessory
Was this helpful?
What can we do to improve the information ?