Technical FAQs

Ask a Question

Is there a way to exclude a POU from being compiled in a SoMachine application.

There is two way for excluding a POU from being compiled.

1) Do no add the POU to the MAST task.
 
2) Right-click on the POU , select Properties and select "Exclude from Build: 
Was this helpful?
What can we do to improve the information ?