Technical FAQs

Ask a Question

Does the M580 BMENOC03x1 ethernet module support the PLC program viewer option.

Yes... Only the M580 BMENOC0311 FactoryCast ethernet module supports the PLC Program Viewer option
Was this helpful?
What can we do to improve the information ?