Technical FAQs

Ask a Question

Can Modbus port #2 be used to flash the executive firmware to a Compact 984?

No, only Modbus port #1 and Modbus Plus can be used to flash the executive firmware to a Compact 984.
Was this helpful?
What can we do to improve the information ?