Technical FAQs

Ask a Question

Can Modbus port #2 be used to flash the executive firmware to a Quantum non Unity PLC?

No, only Modbus port #1 and Modbus Plus can be used to flash the executive firmware to a Quantum non Unity PLC.
Was this helpful?
What can we do to improve the information ?