Technical FAQs

Ask a Question

Can you determine a PLC's Modbus Plus address with Unity Pro?

At this time there is no way to determine a PLC's Modbus Plus address with Unity Pro. There is no feature that will show or adjust the address. 
There is also no System Words (%SW) that hold the address.
Was this helpful?
What can we do to improve the information ?