Technical FAQs

Ask a Question

What is the meaning of the MBP_MSTR error code 16#5068?

Title
MBP_MSTR Opreration 16
 
Issue
MBP_MSTR opreration 16 new error code 16#5068
 
Product Line
Quantum 140NOE771x1
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The MBP_MSTR error code 16#5068 is a new error code added for the use of MBP_MSTR opreration 16 , Reset connections request.
The New MBP_MSTR error 0x5068 means the device has not completed the previous Close connection request.
This happens when sending another Reset connection request before the first Reset connection completes.

 

Was this helpful?
What can we do to improve the information ?