Technical FAQs

Ask a Question

What causes "857 Data Length Mismatch" in Concept?

Issue:
   Error message is displayed when editing Concept project.

Product Line:
    Concept programming software

Resolution:
  • Check if in SFC sections  there are steps with Qualifier and located or unlocated time variables
           - Install patch >B2 or SR2
  • Text compiler was unable to compile a complex logic
             - Simplify the logic.  
  This can happen when combining Projects.
Was this helpful?
What can we do to improve the information ?