Technical FAQs

Ask a Question

Does the Quantum 140NOE771xx Ethernet modules support IP version 6 addressing?

Title
Quantum 140NOE771xx Ethernet modules IP addressing version

Issue
Quantum 140NOE771xx Ethernet modules  IP version 4 addressing

Product Line
Quantum 140NOE771xx
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 No, the Quantum 140NOE771xx Ethernet modules do not support IP version 6 addressing.
The Quantum 140NOE771xx Ethernet modules support only  IP version 4 addressing.

Was this helpful?
What can we do to improve the information ?