Technical FAQs

Ask a Question

Can the Advantys STBAVI1400 module have the channels configured for different voltage ranges?

Yes. You may configure the operating range of the STB AVI 1400 on a per-channel basis.
  • +1 to 5 VDC
  • 0 to 5 VDC
  • 0 to 10 VDC
  • +/-5 VDC
  • +/-10 VDC
Was this helpful?
What can we do to improve the information ?