Technical FAQs

Ask a Question

Can I a Magelis XBTGT communicate to a M221 via the mini-USB port?


The USB port on the M221 cannot be used to communicate with the Magelis HMI like the M340/M580.  The USB port on the M221 does not use the PLC-USB driver and is programming port only.






Was this helpful?
What can we do to improve the information ?