Technical FAQs

Ask a Question

What are the VLAN capabilities of the Connexium TSCESM managed switch?

Title
Connexium TCSESM managed switches and VLANS
 
Issue
Limitations of the Connexium TCSESM managed switches and VLANS
 
Product Line
Connexium TCSESM managed switches
 
Environment
N/A
 
Cause
N/A
 
Resolution
The Maximum number of configurable VLANS is 255. 1. The RSTP protocol only works on VLAN1 and not across multiple VLANS.
The Maximum number of MAC addresss that the TCSESM can store is 1024.
Was this helpful?
What can we do to improve the information ?