Technical FAQs

Ask a Question

Can Unity Pro on Modbus Plus network program through a TCSEGDB23F24FA MB+ Proxy module to an M340 PLC?

Title
Unity Pro programming through a TCSEGDB23F24FA MB+ Proxy
 
Issue
Programming a M340 with Unity Pro through a TCSEGDB23F24FA MB+ Proxy
 
Product Line
M340 TCSEGDB23F24FA Modbus Plus Proxy
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 Yes, a personal computer with the Unity Pro application, that is connected to a Modbus Plus network, can program the M340 that is assigned to the particular TCSEGDB23F24FA Modbus Plus Proxy.
Was this helpful?
What can we do to improve the information ?