Technical FAQs

Ask a Question

Can a M340 be configured to disable the HTTP and FTP access on the CPU Ethernet port?

Title
M340 CPU Ethernet Security
 
Issue
M340 ability to disable the HTTP and FTP access on CPU Ethernet port
 
Product Line
M340 CPU
 
Environment
Unity 8.1
 
Cause
N/A
 
Resolution
The M340 CPU module with firmware release version 2.6 and installation in a Unity 8.1 program gives the user the ability to configure the module for FTP and HTTP Cyber Security capabilities. With this option added a user can prevent FTP/HTTP access to the Ethernet port of the M340 CPU.
In addition the the required module firmware version 2.6 or higher, FTP and HTTP Cyber Security feature requires Unity 8.1 PLC program.
Was this helpful?
What can we do to improve the information ?